Industrial Valves

Introduction Literature FAQ Photos
Industrial Valves
Question: What happened to the code numbers for the WRc approved valves?
Question: What is the difference between direct- and servo-operated solenoid valves?
Question: Which media are your solenoid valves suited for?
Question: I need a spare part for my product. Do you have that?
Question: If my system has back pressure, should I take any precautions?
Question: Where can I find approvals and certificates for Danfoss products? E.g. do you have a PED certificate for KP7W?
Question: Do Danfoss products comply with RoHS directive (Restriction of Hazardous Substances)?
Question: I'm looking for a Danfoss code number and I have not found it in any catalogues?
Question: I need a solenoid valve for a machine for use in North America, do you have some?
Question: I am looking for a Danfoss product, type USC6000, but cannot find it in your catalogues?
Question: Could I send you a Danfoss part for repair?
Question: Do you have a device that cools a heating system on rising temperature?
Question: Which valve should I use for pressure relief function in an open system with high pressure?
Question: Are the code numbers of the EV220B solenoid valves the same as the previous EVSI valves?
Question: I have bought the valve AV210, can you offer me the pilot valve to do the control?
Question: Can I use the EV220B with chlorine?
Question: Which solenoid valve should I choose, if am not sure about the differential pressure of the application?
Question: I am unsure about the pressure conditions in the installation, and I need a solenoid valve, size 1” - which should I choose?
Question: I have installed an pneumatically operated valve type HP210 and it does not work any longer. Can you offer me a new one?
Question: Can I buy Concordia valves?
Question: I am looking for a pump, type APP?
Question: How do I remedy reduced functionality of an AVTA after placing the sensor in a immersion pocket?
Question: Do you have solenoid valves for air compressors?
Question: Is it possible to use AVTA for protecting bio-mass boilers?
Question: I am looking for Danfoss MASSFLO and MAGFLO flow meters?
Question: I am looking for a Danfoss butterfly valve?
Question: Can I use the EV220B solenoid valves for steam applications?
Question: What does it mean that thermostatic valves are proportional and self-acting?
Question: I would like to order a solenoid valve with the stamped no. 446U5252 and can not find it in your system?
Question: Is it possible to replace a copper capillary tube with a stainless steel version?
Question: Does an AVTA valve contain any hazardous parts or substances?
Question: Is it necessary to dismantle AVTA valve from the application to replace the thermostatic element?
Question: Can an AVTA valve be used with glycolic water?
Question: Can I use an AVTA thermostatic valve to regulate air temperature?
Question: Can you deliver your products wordwide?
Question: Do you have a complete catalogue showing all your products?
Question: Can you deliver products exclusively made for us?
Question: Which distribution channels does Danfoss use?
Question: Can I review your stock online?
Question: Where can I find technical drawings of Danfoss products?
Question: What is differential pressure?
Question: What is water hammer?
Question: I need an EV220B 1/2" for an open water system. Which one should I choose?
Question: Can high differential pressure across an AVTA valve influence its functionality?
Question: What does servo-operated mean? Has it to do with servo control?
Question: Can I mount an EV220B valve upside down?
Question: I have mounted an EV220B valve in the warm water circuit of a heating system. The valve does not open. Is it defect?
Question: Is it possible to use the Danfoss solenoid valves on natural gas installations?
Question: I have ordered an EV220B valve NO, but if I blow through the valve, it is closed. Have I got a NC valve?
Question: How can I see if my solenoid valve is NC or NO?
Question: Can I order only the upper part of a valve housing as a spare part?
Question: Where do I direct commercial or technical questions?
Question: What are the difference between direct-, servo- and assisted lift operated valves?
Question: Why does Danfoss not offer EV250B valves in bigger sizes than 1"?
Question: Why is an EV220B solenoid valve more expensive than an EV220A valve?
Question: Do you have local stock?
Question: Why is the sensor mounting position so important for AVTA with universal charge?
Question: Where can we find your data sheets?
Question: Do you have local websites in my language?
Question: Is it possible to place orders online?
Question: Can you give me some key figures on danfoss?
Question: Does Danfoss operate globally?
Question: Is Danfoss a German company?
Question: I am looking for a hydraulic oil pump?
Question: Can we offer a valve according to EN161?
Question: What type of seal material is appropiate for glycol ?
Question: Can I use the EPDM seal material for air?
Question: How can I control air for pneumatically operated valves?
Question: What pressure is required to control AV210 ?
Question: Can I use the AV210 for waste water ?
Question: Can I use an AVTA valve for heating purposes ?
Question: The solenoid valve EV250B is leaking. What should I do?
Question: Is it possible to order a normally open (NO) version of the solenoid valve EV220B 65-100 Cl?
Question: How can I replace 032U7328?
Question: I assemble air suspension system for cars, does Danfoss have any solenoid valve for this kind of application?
Question: I have a Danfoss solenoid valve in NO (normally open) version. Is it possible to change this valve to a NC (normally closed) version?
Question: What is the difference between the AVTA and AVTB ?
Question: What is the difference between the EV220B and EV250B valves?
Question: My AVTA valve's sensor with universal charge is only half immersed in the medium. How does this influence the valve's functionality?
Question: I am looking for a gas valve for Argon application for a closed system, which valve could I use?
Question: What is off-set for thermostatic valves?
Question: What is hysteresis of an AVTA valve?
Question: What is the AVTA valve's reaction time on temperature changes?
Question: Which AVTA valve should I use when the ambient air has H2S, destroying the capillary tube?
Question: What is the compatibility of AVTA body with deionized water, corrosive for metals?
Question: Is there any temperature range preset made for the WVTS valve?
Question: Can you send me a 3.1 certificate for a valve already delivered?
Question: Permissible working pressure for the WVTS valve is 10 bar. What will happen if WVTS will be installed in application where pressure is maximum 16 bar?
Question: How do I see the production date of an AVTA valve?
Question: The pilot unit for WVTS valve is supplied with white plastic washer - is it only packaging protection to be thrown out?
Question: Is it necessary to install a filter ahead of thermostatic valves?
Question: Are AVTA, FJVA and WVTS valves UL or CSA approved?
Question: My WVTS 80 valve has 8 holes for flange connections, but the technical brochure shows only 4. Is the product wrong?
Question: For thermostaticall operated valves, are there any requirements to the cooling water temperature?
Question: My AVTA valves is noisy - why?
Question: How does AVTA react to cooling oil as a medium?
Question: Can AVTA be used for a mixture of alcohol and water?
Question: Is it possible to order a WVTS valve with other charge than universal?
Question: Are thermostatic valves AVTA, FJVA, WVTS normally closed or normally open valves?
Question: The maximum sensor temperature of AVTA (Regulation range 0-30°C) is 57°C. Can the minimum sensor temperature be down to -40°C?
Question: Why is our delivery delayed, when I saw that the delivery date is confirmed for 2 weeks in e-commerce?
Question: Where can I get the technical brochure for AVTA valves?
Question: How do I select the right size AVTA valve?
Question: Are Danfoss AVTA valves UL listed?
Question: What is difference between AVTA and FJVA valves?
Question: Can the sensor element of AVTA valves be installed in any orientation?
Question: Can an AVTA valve be installed in any orientation?
Question: How do I set temperature on AVTA valve?
Question: Where can I find some technical information about your products?
Question: Can I buy a pilot filter separately for flange solenoid valves EV220B 65-100 CI?
Question: Is it possible to install an EV220B (15-50 series) on vertical pipes?
Question: Which solenoid valve should I choose for Glycol as a medium?
Question: I have an EV220B 25B that does not close properly - should I unscrew the equalising orifice to close it?
Question: Can I get an AVTA with ATEX approval?
Question: What do I need to know to select the right product?
Question: Are the solenoid valve Kv values valid for compressed air?
Question: Can I get quality control plans/process flowcharts/material specifications/FMEA for Danfoss products?
Question: Can you send me literature, brochures or catalogues on your products?
Question: I placed an order through e-commerce. Could you please check the delivery dates and inform me the earliest possible delivery?
Question: Which solenoid valve should I choose for showers?
Question: I work with steam and the Danfoss solenoid valve EV225B does not have enough flow. Can you recommend another option?
Question: How do I adjust the temperature on an AVTA valve?
Question: Do you have a solenoid valve for air, 24 V dc and 1/4" thread on both sides?
Question: Can I get Danfoss solenoid valves suitable for seawater?
Question: Can I download product approvals & certificate from the Danfoss websites?
Question: What does "solenoid" mean?
Question: Can I order just the capillary tube for an AVTA?
Question: In a open water system, I have an EV210 valve which does not open - what can be wrong?
Question: Are your valves certificied for use with water?
Question: Could the AV210 capacity control be used together with the AV210 position indicator?
Question: Which media can Danfoss products be used with?